Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

Certified for secure product development

Endress+Hauser receives the IEC 62443-4-1 certification, thus laying a further building block for compliance with the European Cyber Resilience Act.

Fecha de publicación: 31.10.2024

In October 2024, TÜV Rheinland, the German Technical Inspection Association in the Rhineland region of Germany, certified the secure product development process at Endress+Hauser in accordance with the IEC 62443-4-1 security standard, maturity level 3. Five product centers have received the certification and thus meet the requirements for the life cycle of the products.

The Council of the European Union passed the Cyber Resilience Act (CRA) in October 2024. This stipulates that products must demonstrate a high level of cybersecurity throughout their entire life cycle. Appropriate measures and methods must be implemented as early as the product development stage. Endress+Hauser follows this “Security by Design” approach to provide customers with the best possible support in protecting their systems. 

“We are particularly proud of this certificate as it recognizes our many years of effort to achieve the highest level of security in our product centers. This level of structured approach across many different development sites shows the importance Endress+Hauser places on cybersecurity,” says Mirko Brcic, Product Security Officer at Endress+Hauser.

One visible result of the cybersecurity measures is the development of secure access to Endress+Hauser measuring devices via Bluetooth. Even the internet standardization body IETF now recommends the CPace protocol used in the Endress+Hauser SmartBlue app for password-protected access.

Standard affects various aspects

In principle, a company that aligns its processes with IEC 62443-4-1 must prove that cybersecurity is incorporated throughout the entire life cycle of a product. As part of the group certification, the certifying body checks the following aspects, among others:

  • Risk and threat analyses

  • Security by design

  • Security testing

  • Vulnerability management

  • Customer security manual

“With the IEC 62443-4-1 certification, we have jointly laid the foundation for supplying secure products in the future and being prepared for regulations such as the CRA,” says Mr Brcic. Five of the Group’s competence centers were certified: Endress+Hauser Flow, Endress+Hauser Level+Pressure, Endress+Hauser Liquid Analysis, Endress+Hauser Temperature+System Products, and Endress+Hauser Digital Solutions. 

Descargas

    EH_2024-10-31_IEC-62443-4-1.zip

Press list

Reciba los próximos comunicados de prensa y noticias directamente en su bandeja de entrada. Asegúrese de estar al día y suscríbase al listado de prensa de Endress+Hauser.

Lista de prensa de Endress+Hauser

Endress+Hauser envía periódicamente comunicados de prensa sobre temas actuales e información de la compañía a los profesionales de los medios de comunicación.

Seleccione los temas que le interesan:  *
Seleccione las industrias que le interesan: *

Datos personales

Los campos marcados con un asterisco (*) son obligatorios. Recibirá un mensaje de correo electrónico con la confirmación de su suscripción. La información proporcionada es voluntaria y sus datos solo se usarán para personalizar los boletines informativos y no se transferirán a terceras partes. Por razones estadísticas, realizaremos un seguimiento anónimo de los enlaces.

Contacto